SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
The MCU GPIO is a general-purpose input/output module that allows software to write to and read from the DIOs. These pins are configured by the IOC module. To modify a single GPIO output value, use the GPIO.DOUTn registers. The following describes the necessary steps to set up DIO1 as a GPIO output and toggle the bit.
TI recommends using the GPIO driver in the SimpleLink™ Low Power F3 Software Development Kit (SDK) when managing general purpose I/Os.