SPRUJ64 September 2022
To identify the version of the board, an M1 sticker is pasted on the top side of the board, as shown in Figure 2-2. The M1 sticker on the board signifies that R302 and C294 are not assembled (DNI) on the board.