SPRUJ64 September 2022
The SKEVM receives 5-V input from a USB Type-C connector. The following sections describe the power distribution network topology that supply the SKEVM board, supporting components and reference voltages.
The AM64x SKEVM board includes a power solution based on PMIC and a few discrete regulators. The initial stage of the power supply is 5 V from a Type-C USB connector with part No 2012670005 from Molex, which supports a 3A current rating and necessary protection circuits for over current and voltage surge. The 5-V input (VUSB_MAIN) from the USB Connector is used to generate 3.3 V (VCC3V3SYS_EXT) with the help of switching regulator (part No. LM61460AASQRJRRQ1), which is the input supply to the PMIC section. PMIC generates the necessary voltages required for the SKEVM.
A Toggle switch (with part number AS11AP) is provided to initiate the power on and power down sequence of the Board. This switch connects TPS6522053_EN enable signal to ground when switch is in OFF position and enables PMIC TPS6522053RHBR when the switch is in ON position, thereby initiating the Power – Up Sequence. A low on enable pin of the TPS6522053RHBR PMIC, by sliding the switch to OFF position, initiates the Power-down sequence.
Additionally, TEST_POWERDOWN from the test automation header is also connected to the enable pin of TPS6522053RHBR PMIC to control on/off of the EVM through the test automation board. The test automation connector requires 3.3-V supply, which is provided from power mux (part No: TPS2121RUXT). The inputs to the power mux are 3V3 from two different sources. First 3V3 supply is generated from 5V (XDS_USB_VBUS) using an LDO (Part No: TPS79601DRBR). This will be generated if the Micro B cable is connected to J12. Second 3V3 input is generated from 5V (VUSB_MAIN) using a switching Buck regulator (part No: TPS62177DQCR). This is an Always ON Regulator and supplies the necessary power if the USB Type C Cable is plugged in. When Both Type C cable and Micro B cable at J12 are connected, the mux priority is set to its first input supply (VCC3V3_XDS). If USB is not connected to the J12, the mux output is from VCC3V3_TA, which is an always ON power supply.