SPRUJ64 September 2022
There are 8 LEDs connected to an I2C-based LED driver (TPIC2810D), which is controlled by the SoC through the I2C1 port. These 8 LEDs can be toggled based on the user application. Primarily these eight LEDs are meant for Industrial application.
Figure 4-16 Ethernet
Interface - LEDs