SLUUCP8A June 2024 – April 2025 BQ41Z50
This command enables/disables firmware-based fuse activation to ease testing during manufacturing. The initial setting is loaded from Mfg Status Init[FUSE_EN]. If the ManufacturingStatus()[FUSE_EN] = 0, sending this command allows the FW to control the FUSE output and the ManufacturingStatus()[FUSE_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[FUSE_EN] status is copied to Mfg Status Init[FUSE_EN] when the command is received by the gauge. The BQ41Z50 device remains on its latest Fuse Control setting prior to a reset.