| RSVD (Bits 7–2): Reserved. Do not use. |
| | |
| ISTORE_RM (Bit 1): This bit defines whether the stored value of RM (IATA RM) or the true value is displayed during the IATA Delay Time period. |
| 1 = | Stored value of RM (IATA RM) is displayed during the IATA Delay Time period. (default) |
| 0 = | True (present) value of RM is displayed. |
| | |
| ISTORE_FCC (Bit 0): This bit defines whether the stored value of FCC (IATA FCC) or the true value is displayed during the IATA Delay Time period. |
| 1 = | Stored value of FCC (IATA FCC) is displayed during the IATA Delay Time period. (default) |
| 0 = | True (present) value of FCC is displayed. |