SLUUCP8A June 2024 – April 2025 BQ41Z50
To reduce power consumption, the device can be sent to SHUTDOWN mode before shipping. After sending this command, the OperationStatus()[SDM] = 1, an internal counter will start, and the CHG and DSG FETs will be turned off when the counter reaches Ship FET Off Time. The counter will continue to count up after the FETs are turned off. When the counter reaches Ship Delay time, the device will enter SHUTDOWN mode if the voltage at PACK pin is < Shutdown Voltage and no charger present is detected.
If the device is SEALED, this feature requires the command to be sent twice in a row within 4 seconds (for safety purposes). If the device is in UNSEALED or FULL ACCESS mode, sending the command the second time will cancel the delay and enter shutdown immediately.
To wake up the device, a voltage > Charger Present Threshold must apply to the PACK pin. The BQ41Z50 device will power up and a full reset is applied.