SWRA751 September 2022
Description:
This command starts the A2DP data streaming to the remote device. The host should initiate PCM audio data right after this API call. When no PCM data is accepted at the controller after this command call, no data will be sent to the peer device.
| Command Parameter | Size (bytes) | Value | Description |
|---|---|---|---|
| Connection handle | 1 | 0x1 - 0x7 | The ACL connection handle |
| Reserved | 4 | For future use |
| Returned Value | Description | Size (bytes) | Events Generated |
|---|---|---|---|
| 0x00 0x01 – 0xFF |
Command succeeded. Command failed. |
1 | Command Complete |