SWRA751 September 2022
Description:
This command enables an RF calibration run immediately or periodically. It defines the calibration procedures required to run each time the periodic calibration is run. In standby mode, when enabling the periodic run, the calibration should start the run immediately.
| Command Parameter | Size (bytes) | Value | Description |
|---|---|---|---|
| Periodic mode | 1 |
0x00 0x01 - 0xFD 0xFE 0xFF |
Activate the calibration one time Activate the calibration each Value × 10 seconds periodically Do not change Stop the periodic calibration |
| Calibration procedures | 4 | 0xXXXXXXXX | Default: 0xFFFFFFFF |
| Override temp condition | 1 |
0x00 0x01 |
Activate the calibrations only if the temperature has changed. Activate the calibrations at every periodic calibration. |
| Returned Value | Description | Size (bytes) | Events Generated |
|---|---|---|---|
| 0x00 0x01 – 0xFF |
Command succeeded. Command failed. |
1 | Command Complete |