SWRA751 September 2022
Description:
Some Bluetooth devices do not support the power control feature, which allows increasing or decreasing the transmitted power level of the other devices in the connection. This command lets the user set the power level to be used during such a connection, so that the fixed power does not compress the other receiver. This is done by selecting from the 16 available power levels. The device then transmits at this level all the time. This single power can be set per modulation scheme.
| Command Parameter | Size (bytes) | Value | Description |
|---|---|---|---|
| GFSK single power level Status | 1 | 0 to 150xFF | Sets the GFSK power level to be
used without power control Don’t change. |
| EDR2 single power level | 1 | 0 to 150xFF | Sets the EDR2 power level to be
used without power control Don't change. |
| EDR3 single power level | 1 | 0 to 150xFF | Sets the EDR3 power level to be used without power control. |
| Returned Value | Description | Size (bytes) | Events Generated |
|---|---|---|---|
| 0x00 0x01 – 0xFF |
Command succeeded. Command failed. |
1 | Command Complete |