SLVUCU5 December 2025 UCD91160 , UCD91320
The Manufacturer Status bits are defined in Table 26-34. With the exception of the STORE_DEFAULT_ALL_DONE bit, whenever any of these bits are set, the PMBALERT# line is asserted.
| Byte Number (write) | Byte Number (Read) | Payload Index | Bit in Each Payload Byte | Name | Descriptions |
|---|---|---|---|---|---|
| 0 | CMD = F3 | ||||
| 1 | 0 | BYTE_COUNT = 6 | |||
2 | 1 | 0 | 0 | GPI25 Fault | Set whenever the GPI is de-asserted |
... | ... | ... | ... | ... | ... |
2 | 1 | 0 | 7 | GPI32 Fault | |
3 | 2 | 1 | 0 | GPI17 Fault | |
... | ... | ... | ... | ... | |
3 | 2 | 1 | 7 | GPI24 Fault | |
4 | 3 | 2 | 0 | GPI9 Fault | |
... | ... | ... | ... | ... | |
4 | 3 | 2 | 7 | GPI16 Fault | |
5 | 4 | 3 | 0 | GPI1 Fault | |
... | ... | ... | ... | ||
5 | 4 | 3 | 7 | GPI8 Fault | Set whenever the GPI is de-asserted |
6 | 5 | 4 | 0 | WATCHDOG_TIMEOUT | A UCD91xxx internal watchdog timeout reset has occurred |
1 | STORE_DEFAULT_ALL_DONE | The STORE_DEFAULT_ALL operation has completed | |||
2 | STORE_DEFAULT_ALL_ERROR | An error occurred during STORE_DEFAULT_ALL | |||
3 | SYSTEM_WATCHDOG_TIMEOUT | A system watchdog timeout reset has occurred (see Section 26.5) | |||
4 | NEW_ LOGGED_FAULT_DETAIL | This bit is set whenever a new fault detail entry is logged. It is cleared whenever the LOGGED_FAULT_DETAIL command is read. | |||
5 | STORE_PARM_VALUE_ERROR | An error occurred during downloading the configuration | |||
6 | SINGLE_EVENT_UPSET | Single event upset occurred | |||
7 | LFCLK_FAILURE | A failure of the low frequency clock used for the RTC has occured. This is only relevant when the LFCLK enable bit is set in the MISC_CONFIG command. | |||
7 | 6 | 5 | 0 | SLAVED_FAULT | The rail was shutdown because it is dependent on another rail that had a fault (paged) [See Section 26.36.9] |
1 | SEQ_ON_TIMEOUT | Sequence on timeout (paged) [See Section 26.36.4] | |||
2 | SEQ_OFF_TIMEOUT | Sequence off timeout (paged) [See Section 26.36.4] | |||
3 | HARDCODED_PARMS | PMBus hard-coded configuration values have been loaded into RAM. The data flash image on the device is empty or corrupt. This state is referred to as a NOBOARD configuration. This default configuration only minimally configures the device (for example, no rails are defined). Executing a STORE_DEFAULT_ALL command updates the data flash on the device. After a STORE_DEFAULT_ALL and reset, this HARDCODED_PARMS status bit is cleared. It also can be cleared with the CLEAR_FAULTS command. | |||
4 | PKGID_MISMATCH | Hardware Package ID does not match firmware | |||
5 | RESEQUENCE_ERROR | An error occurred during the re-sequencing operation. This occurs when one of the rails that are part of the resequence operation does not turn off before its TOFF_MAX_WARN_LIMIT. | |||
6 | LOGGED_FAULT_DETAIL_FULL | The LOGGED_FAULT_DETAIL buffer is full [See Section 26.26 ) | |||
7 | INVALID_LOG | A checksum match failed for a log during non-volatile memory check. |