SLVUCU5 December 2025 UCD91160 , UCD91320
The PMBus specification uses the same term, linear, to describe both the 16-bit+exponent format used for the voltage-related parameters as well as the 11-bit+exponent format used for other parameters. In cases where it is necessary to distinguish between these two data formats, this document uses the term LINEAR16 or LINEAR11.