SLVUCU5 December 2025 UCD91160 , UCD91320
This configures the output pin (see Section 23). This pin is asserted if the system watchdog’s timeout counter does not receive reset signal or command within the time period defined by the Reset Period byte.