SLVUCU5 December 2025 UCD91160 , UCD91320
The bit definitions for common faults are shown in Table 26-25.
By examining this single bit (bit 0 of the Non-Paged Faults byte), a host can determine if any page-dependent or GPI faults have occurred. A value of 0 in this bit indicates that all of the page-dependent and GPI fault log entries are 0 and need not be read. A value of 1 in this bit indicates that one or more of the page-dependent, or GPI faults has occurred. In that case, the host must examine all of the log entries to determine which ones have log information.
| Bit | Description | Can Generate a LOGGED_FAULT_DETAIL Entry? |
|---|---|---|
| 0 | LOG_NOT_EMPTY | No |
| 1 | System Watchdog Timeout | Yes |
| 2 | Resequence Error | No |
| 3 | Watchdog Timeout | Yes |
| 4 | Reserved | No |
| 5 | Reserved | No |
| 6 | Reserved | No |
| 7 | Reserved | No |