SLVUCU5 December 2025 UCD91160 , UCD91320
When this bit is set, a system watchdog timeout causes the reset pin to be asserted for the time identified by the Delay Time.
If the “Watchdog Timeout Assertion Uses GPI Tracking Release Delay” bit is set, the GPI Tracking Release Delay is used instead of the Delay Time.