SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
The Flash Wrapper checks the user-provided data during program command execution. Specifically, this data validity check looks for a bit in the targeted flash words that is already programmed to 0 and is configured by the current operation to be programmed to a 1. Programming an existing 0 to a 1 in the Flash is not possible. If such a condition is detected, then the program operation terminates with a FAILINVDATA error in STATCMD without issuing the programming command.