SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ
At the end of all command executions in the Flash Wrapper, several registers are forced back to the default states. This default state usually allows protection from program or erase without an update to the MMR. For example, CMDWEPROT* defaults to protect all sectors, which means neither a program nor an erase can be done without clearing the bit (or bits) of the targeted sector. Also, the data buffer registers of the program command inside the Flash wrapper default to all 1s, which means the registers must be updated to do a program operation.