SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ
When a node on the CAN network receives a transmitted message, the CAN network sends an acknowledgment that the message was successfully received. When a transmitted message is not acknowledged by the recipient node, the transmitting CAN flags an acknowledge error. Error response and any necessary software requirements are defined by the system integrator.