SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
ePWM modules can be chained together using a clock synchronization scheme that allows the modules to operate as a single system when required. In the synchronous mode of operation, checking for proper synchronization of the various PWM instances is critical to avoid catastrophic conditions. The synchronization of the various PWMs can be checked by reading the TBSTS.SYNCI bit of the ePWM module. The correct phase relationship that is intended as a result of the sync operation can be crosschecked by comparing the TBCTR register value.