SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ
The link pointer OTP location is not protected by ECC. Majority voting and data-consistency-based error detection is implemented to provide better security to the customer code and enable application safety. The location of the zone-select region in OTP is decided based on the value of three 29-bit link pointers (Zx-LINKPOINTERx) programmed in the OTP of each zone of each CPU subsystems. The final value of the link pointer is resolved in hardware when a dummy read is issued to all the link pointers by comparing all the three values (bit-wise voting logic). Any error in the resolution of the final link pointer value sets the Zx_LINKPOINTERERR register.