SFFS779 December 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
In the CAN message protocol, several of the frame segments are coded through bit stuffing. Whenever a transmitter detects five consecutive bits of identical value in the bit stream to be transmitted, the CAN message protocol automatically inserts a complementary bit into the actual transmitted bit stream. If a sixth consecutive equal bit is detected in a received segment that should have been coded by bit stuffing, the CAN module flags a stuff error. Error response and any necessary software requirements are defined by the system integrator.