ZHCSL05C October 2019 – October 2023 TPS65313-Q1
PRODUCTION DATA
The device has two general-purpose supply voltage monitors at the EXT_VSENSE1 and EXT_VSENSE2 pins. The nominal voltage level at the pins must be set to 0.8 V by the external resistor divider as shown in Figure 11-31. Each monitor detects undervoltage and overvoltage events. These events set the corresponding status bit in the EXT_VMON_STAT register. The TPS65313-Q1 device can be factory-programmed such that each monitor is either enabled or disabled during a device start up (NPOR) event. If either of the voltage monitors is programmed to be enabled during an NPOR event, the voltage monitor does not detect an undervoltage event before the RESET extension starts. After the device goes to the DIAGNOSTIC state, the system MCU can set the EXT_VMONx_EN control bits in the PWR_CTRL register to either enable or disable the voltage monitors. When these bits are set by the MCU, the bits stay unchanged when the device goes into the RESET state for any reason.
A corresponding UV flag in the EXT_VMON_STAT register is set after a power-up (NPOR) event, if the external supply voltage at the EXT_VSENSEx pin was below its undervoltage threshold, and when the voltage monitor was enabled. The device goes into the OFF state, if the external supply does not reach the target regulation voltage within the tRESET_STATE_TO time, and after the voltage monitor was enabled.
The device response to fault detection from the monitors is configured by writing the desired data to the EXT_VMON1_CFG and EXT_VMON2_CFG registers.
Figure 11-31 External VSENSEx