SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
To setup the channel filters in LGPT follow these steps:
When configuring the channel filter make sure the channel filter period is not shorter than the timer clock period. That is,
(Channel filter clock period) x (CHFILT.LOAD) > timer clock period.
If this is not satisfied capture events can be missed.