SPMU447 June 2026 CC2755P20
The following sequence is executed by the system CPU to perform an APU operation:
Transfer the input data into the APU data memory
Initiate the required operation by calling the API
Receive an interrupt request (IRQ) from the APU when the API has completed its operation
Read the result data from the APU data memory