SPMU447 June 2026 CC2755P20
Verify the specified parts of the flash SCFG sector, using CRC32.
The SCFG is covered by a single CRC which spans from the first field to the Scfg.res0 field
The commands perform one of these checks:
The command result shall be SUCCESS if all performed checks are successful.
These conditions must be true:
| Word | Bits | Field | Value | Description |
|---|---|---|---|---|
0 | 7:0 | cmdId | 0x1B | Command ID |
15:8 | respSeqNumber | User defined | Optional response sequence number, included in the response header | |
16 | checkExpCrcs | - | Check SCFG data also against the expected CRC32 fields the command:
| |
31:17 | reserved0 | 0x00 | Reserved | |
1 | 31:0 | expCrc32 | - | Expected CRC32 of the SCFG:
|
| Word | Bits | Field | Value | Description |
|---|---|---|---|---|
0 | 7:0 | cmdId | 0x1B | Command ID, copied from the first command parameter word |
15:8 | respSeqNumber | User defined | Optional sequence number, copied from the first command parameter word | |
23:16 | result | - | Command result. One of the common results, or:
| |
31:24 | dataWordCount | 0 | Size of additional response data, in number of 32-bit words |
These checks are performed before command execution, in the indicated order:
If any restriction is violated: Fail with result NOT_ALLOWED