Secure Boot will enter ROM Panic mode if it is determined that there are no targets that can be booted. The following is a list of steps for System ROM to perform when it determines that the boot sequence cannot proceed:
Isolate (decouple) main flash, so that the flash
cannot be written / read.