SPMU447 June 2026 CC2755P20
There are six peripheral subscribers for the MCU event fabric. These subscribers are different peripherals that must be configured differently according to the purpose of those specific peripherals. The following subscribers are not described in this chapter, but rather in each of the corresponding peripheral chapters:
The following two subscribers are described below: