SPMU447 June 2026 CC2755P20
This command is used to tell the bootloader to reset. This is used after downloading a new image to the device to cause the new application to start from a reset. The normal boot sequence occurs and the image runs as if from a hardware reset. This command can also be used to reset the bootloader if a critical error occurs and the host device wants to restart communication with the bootloader.
The bootloader responds with an ACK signal to the host device before actually executing the system reset of the device running the bootloader. This informs the updater host device that the command was received successfully and the part will be reset.
| Byte | Field | Description |
|---|---|---|
| 0 | cmdId | BLDR_CMD_RESET command ID |