SPMU447 June 2026 CC2755P20
The DSSM provides four interrupt sources that can be configured to source a CPU interrupt event. The CPU interrupt events from the DSSM are given in Table 5-6.
| Name | Description |
|---|---|
| TXIFG | Indicates that the TX_DATA buffer in the DSSM has received data. |
| RXIFG | Indicates that the data in RX_DATA buffer in the DSSM was read. |
| PWRUPIFG | Indicates that the DEBUGSS was started due to a debug probe attaching to the device. |
| PWRDWNIFG | Indicates that the DEBUGSS was stopped due to a debug probe disconnecting from the device. |
See Chapter 4 for guidance on configuring the DEBUGGSS event as a CPU interrupt.