SPMU447 June 2026 CC2755P20
A capture request signal can be routed from RFCORE to trigger samplestamp capture. Whenever the event - samplestamp request(pulse detection inside the IP) signal is high:
The current value of STMPXCNT is copied into STMPXCNTCAPT0.
The current value of STMPWCNT is copied into STMPWCNTCAPT0.
Also, on the first WCLK edge of each frame, the current value of STMPXCNT is captured in STMPXPER, and STMPXCNT then restarts counting from 0.
Using these values, a fixed-point samplestamp value can be calculated:
STMPWCNTCAPT0 + (STMPXCNTCAPT0 / STMPXPER)
Notice that the value of STMPXPER will not normally be captured at the same time as the other values. Therefore, STMPXPER can be less than STMPXCNTCAPT0.