SPMU447 June 2026 CC2755P20
The lowest power state of the device, RESET, is entered unconditionally when the reset pin is held low. In this state, no oscillators are running, all voltage regulators are disabled and I/Os have both their input and output buffers disabled. There is no internal mechanism to allow software to enter RESET, nor any software mechanism to allow exit from RESET. Thermal shutdown functionality, after being explicitly triggered by software, holds the device in the RESET state by pulling the RSTN pin low as long as the temperature is above the set threshold. See the device-specific data sheet for thermal threshold values.