SLUUDA0 April 2026 BQ27Z855
This command returns the cell voltages, PACK voltage, BAT voltage, cell currents, cell powers, power, and average power on ManufacturerBlockAccess() or ManufacturerData().
| Status | Condition |
|---|---|
| Activate | 0x0071 to ManufacturerBlockAccess() or ManufacturerAccess() |
Action: Output 32 bytes of data on ManufacturerBlockAccess() or ManufacturerData() in the following format: aaAAbbBBccCCddDDeeEEffFFggGGhhHHiiIIjjJJkkKKllLLmmMMnnNNooOOppPP where:
| Value | Description | Unit |
|---|---|---|
| AAaa | Cell Voltage 1 | mV |
| BBbb | RSVD - Do not use | mV |
| CCcc | RSVD - Do not use | mV |
| DDdd | RSVD - Do not use | mV |
| EEee | RSVD - Do not use | mV |
| FFff | PACK voltage. Voltage at the PACK+ pin. | mV |
| GGgg | Cell Current 1. Simultaneous current measured during Cell Voltage 1 measurement | mA |
| HHhh | RSVD - Do not use | mA |
| IIii | RSVD - Do not use | mA |
| JJjj | RSVD - Do not use | mA |
| KKkk | Cell Power 1. Calculated using Cell Voltage1 and Cell Current 1 data | cW |
| LLll | RSVD - Do not use | cW |
| MMmm | RSVD - Do not use | cW |
| NNnn | RSVD - Do not use | cW |
| OOoo | Power calculated by Voltage() × Current() | cW |
| PPpp | Average Power | cW |