ZHCSB17D february 2013 – july 2023 TUSB8040A1
PRODUCTION DATA
The TUSB8040A1 supports per port or ganged power switching and over-current protection.
An individually port power controlled hub switches power on or off to each downstream port as requested by the USB host. Also when an individually port power controlled hub senses an over-current event, only power to the affected downstream port will be switched off.
A ganged hub switches on power to all its downstream ports when power is required to be on for any port. The power to the downstream ports is not switched off unless all ports are in a state that allows power to be removed. Also when a ganged hub senses an over-current event, power to all downstream ports will be switched off.
The TUSB8040A1 also provides customization using an I2C EEPROM or configuration via an SMBus host for vendor specific PID, VID, and strings. For the TUSB8040A1 ports can also be marked as disabled or permanently attached using pin selection, I2C EEPROM or an SMBus host. The Device Status and Command Register at F8h cannot be modified by the contents of the I2C EEPROM.