选择版本
SMARTRFTM-STUDIO
SmartRF Studio
Zip file with Windows Installer and SW Manifest
产品
MSP430 微控制器
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
Sub-1GHz 收发器
其他无线产品
汽车类无线连接产品
硬件开发
文档
Compressed source file archive
发布信息
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
最新动态
- [CC1352P] The Code Export feature has been updated to support the RF Command structure used for programming of High TX power output (High PA).
- Two methods to program the High TX power output are supported, the "normal" method and the "Legacy" method. The "Legacy" method is deprecated and will be removed in the future (SRFSTUDIO-1459).
- [CC13x2R/P] Radio settings (Preview): New settings for the 863-930 MHz band. 200kbps, 2-GFSK, 50 kHz deviation PHY (SRFSTUDIO-1511, SRFSTUDIO-1522).
- [CC13x0] Radio settings : New settings for the 863-930 MHz band. WB-DSSS: Wideband Direct Sequence Spread Spectrum (SRFSTUDIO-1509).
- [CC13x0] Radio settings : New settings for the 430-520 MHz band. OOK, 4.8 kbps (SRFSTUDIO-1799).
- [CC13x0] Code export for CC13x0 devices is no longer compatible with SimpleLink TI-RTOS v2.2x due to a API definition mismatch in command CMD_PROP_RADIO_SETUP.
- As a consequence, template "default_tirtos_template" has been removed for these devices (SRFSTUDIO-1864).
- [CC2654] Device icon has been removed from the Startup Window because the CC256x Bluetooth Hardware Evaluation Tool is no longer available from TI.com (SRFSTUDIO-1841).