SPRUI04E July 2015 – January 2023
This document uses the following conventions:
special typeface
. Interactive
displays use a bold version of the special typeface to distinguish commands that you enter
from items that the system displays (such as prompts, command output, error messages,
etc.). Here is a sample of C code:
#include <stdio.h>
main()
{ printf("Hello World\n");
}
cl6x [options] [filenames] [--run_linker [link_options] [object files]] |
cl6x --run_linker {--rom_model | --ram_model} filenames [--output_file= name.out] | |
--library= libraryname |
symbol .usect "section name", size in bytes[, alignment] |