SPRUI04E July 2015 – January 2023
In the C++ program in Section 9.7.2.1, the extern declaration of asmfunc is optional because the return type is int. Like C/C++ functions, you need to declare assembly functions only if they return noninteger values or pass noninteger parameters.
SP Semantics
The stack pointer must always be 8-byte aligned. This is automatically performed by the C compiler and system initialization code in the run-time-support libraries. Any hand-written assembly code that has interrupts enabled or calls a function defined in C or linear assembly source should also reserve a multiple of 8 bytes on the stack.
Stack Allocation
Even though the compiler guarantees a doubleword alignment of the stack and the stack pointer (SP) points to the next free location in the stack space, there is only enough guaranteed room to store one 32-bit word at that location. The called function must allocate space to store the doubleword.
Alignment of __x128_t Type Data Objects (C6600 Only)
The C6600 provides the 128-bit container type __x128_t. Global data objects of this type are aligned to an 16-byte boundary (128 bits). Local __x128_t variables are allocated on the stack, but are not necessarily aligned on an 16-byte boundary, since their actual alignment depends on the alignment of the stack pointer (SP) and the SP-relative offset of the local __x128_t type object. The compiler aligns the stack to an 8-byte boundary.