SPRUI04E July 2015 – January 2023
Another aspect of the unordered() operator that should be taken into consideration is that even though the operator causes the linker to relax constraints imposed by the explicit specification of an output section's contents, the unordered() operator will still respect the position of a dot (.) expression within such a specification.
Consider the output section specification in Section 5.12.7.3.1.