SPRUI04E July 2015 – January 2023
Assign a Variable to a Register in a Set
.pref symbol / register1 [/register2...]
The .pref directive communicates a preference to assign a variable to one of a list of registers. The preference is used only in the .cproc or .proc region the .pref directive is declared in and is valid only until the end of the region.
symbol | A valid symbol name to be assigned to the register. The substitution symbol is up to 128 characters long and must begin with a letter. Remaining characters of the symbol can be a combination of alphanumeric characters, the underscore (_), and the dollar sign ($). | |
register | List of actual registers to be assigned a variable. |
There is no guarantee that the symbol will be assigned to any register in the specified group. The compiler may ignore the preference.
When a symbol is declared with the .pref directive, it is not necessary to declare that variable with the .reg directive.
Here x is given a preference to be assigned to either A6 or B7. However, It would be correct for the compiler to assign x to B3 (for example) instead.
.PREF x/A6/B7 ; Preference to assign x to either A6 or B7