SPRUI04E July 2015 – January 2023
Following are detailed descriptions of options that you will probably use frequently:
--c_src_interlist | Invokes the interlist feature, which interweaves original C/C++ source with compiler-generated assembly language. The interlisted C statements may appear to be out of sequence. You can use the interlist feature with the optimizer by combining the --optimizer_interlist and --c_src_interlist options. See Section 5.17. The --c_src_interlist option can have a negative performance and/or code size impact. |
--cmd_file=filename | Appends the contents of a
file to the option set. Use this option to avoid
limitations on command line length or C style
comments imposed by the operating system. Use a #
or ; at the beginning of a line in the command
file to include comments. You can add comments by
surrounded by /* and */. To specify options,
surround hyphens with quotation marks. For
example, "--"quiet. You can use the --cmd_file
option multiple times to specify multiple files.
For example, the following indicates file3 should
be compiled as source and file1 and file2 are
--cmd_file
files:
|
--compile_only | Suppresses the linker and overrides the --run_linker option, which specifies linking. The --compile_only option's short form is -c. Use this option when you have --run_linker specified in the C6X_C_OPTION environment variable and you do not want to link. See Section 7.2.3. |
--define=name[=def] | Predefines the constant
name for the preprocessor. This is
equivalent to inserting #define name def at
the top of each C source file. If the
optional[=def] is omitted, the name
is set to 1. The --define option's short form is
-D. If you want to define a quoted string and keep the quotation marks, do one of the following:
|
--help | Displays the syntax for invoking the compiler and lists available options. If the --help option is followed by another option or phrase, detailed information about the option or phrase is displayed. For example, to see information about debugging options use --help debug. |
--include_path=directory | Adds directory to the list of directories that the
compiler searches for #include files. The --include_path option's short form is
-I . You can use this option several times to define several
directories; be sure to separate the --include_path options with spaces. If you do
not specify a directory name, the preprocessor ignores the --include_path option.
See Section 4.6.2.1. |
--keep_asm | Retains the assembly language output from the compiler or assembly optimizer. Normally, the compiler deletes the output assembly language file after assembly is complete. The --keep_asm option's short form is -k. |
--quiet | Suppresses banners and progress information from all the tools. Only source filenames and error messages are output. The --quiet option's short form is -q. |
--run_linker | Runs the linker on the specified object files. The --run_linker option and its parameters follow all other options on the command line. All arguments that follow --run_linker are passed to the linker. The --run_linker option's short form is -z. See Section 7.2. |
--skip_assembler | Compiles only. The specified source files are compiled but not assembled or linked. The --skip_assembler option's short form is -n. This option overrides --run_linker. The output is assembly language output from the compiler. |
--src_interlist | Invokes the interlist feature, which interweaves optimizer comments or C/C++ source with assembly source. If the optimizer is invoked (--opt_level=n option), optimizer comments are interlisted with the assembly language output of the compiler, which may rearrange code significantly. If the optimizer is not invoked, C/C++ source statements are interlisted with the assembly language output of the compiler, which allows you to inspect the code generated for each C/C++ statement. The --src_interlist option implies the --keep_asm option. The --src_interlist option's short form is -s. |
--tool_version | Prints the version number for each tool in the compiler. No compiling occurs. |
--undefine=name | Undefines the predefined constant name. This option overrides any --define options for the specified constant. The --undefine option's short form is -U. |
--verbose | Displays progress information and toolset version while compiling. Resets the --quiet option. |