SPRUI04E July 2015 – January 2023
In Section 5.12.7.3.1, a dot (.) expression, ". += 0x100;", separates the explicit specification of two groups of functions in the output section. In this case, the linker will honor the specified position of the dot (.) expression with respect to the functions on either side of the expression. That is, the unordered() operator will allow the preferred function order list to guide the placement of func_a through func_d relative to each other, but none of those functions will be placed after the hole that is created by the dot (.) expression. Likewise, the unordered() operator allows the preferred function order list to influence the placement of func_e through func_h relative to each other, but none of those functions will be placed before the hole that is created by the dot (.) expression.