SPRUI04E July 2015 – January 2023
advice #30011: Consider adding assertions to indicate n-byte alignment
of variables input1, input2, output if they are actually n-byte
aligned: _nassert((int)(input1) % 8 == 0).
Most loops have memory access instructions. The compiler attempts to use wider load instructions, and aligned memory accesses instead of non-aligned memory accesses to reduce/balance out resources used for the memory access instructions. One of the ways to let the compiler know that it is safe to use "wider" loads is to use the keyword "_nassert".
To find out more on using the _nassert keyword, see Section 9.7.11.