SPRUI04E July 2015 – January 2023
If you are using C++, there are several TI-specific attributes that can be applied to loops. No corresponding syntax is available in C. The following TI-specific attributes have the same function as their corresponding pragmas:
See Section 8.10.22.1 for an example that uses a for loop attribute.