SPRUI04E July 2015 – January 2023
You can use the .mdep directive to identify specific memory Dependencies by annotating each memory reference with a name, and using those names with the .mdep directive to indicate the actual dependence. Annotating a memory reference requires adding information right next to the memory reference in the assembly stream. Include the following immediately after a memory reference:
{ memref}
The memref has the same syntax restrictions as any assembly symbol. (For more information about symbols, refer to the TMS320C6000 Assembly Language Tools User's Guide.) It is in the same name space as the symbolic registers. You cannot use the same name for a symbolic register and annotating a memory reference.