SPRUI04E July 2015 – January 2023
The following options are used to select symbolic debugging or profiling:
--profile:breakpt | Disables optimizations that would cause incorrect behavior when using a breakpoint-based profiler. |
--symdebug:dwarf | (Default) Generates directives that are used by the C/C++ source-level debugger and enables assembly source debugging in the assembler. The --symdebug:dwarf option's short form is -g. See Section 5.18. For details on the DWARF format, see The DWARF Debugging Standard. |
--symdebug:dwarf_ version={2|3} | Specifies the DWARF debugging format version (2 or 3) to be generated when --symdebug:dwarf (the default) is specified. By default, the compiler generates DWARF version 3 debug information. For more information on TI extensions to the DWARF language, see The Impact of DWARF on TI Object Files (SPRAAB5). |
--symdebug:none | Disables all symbolic debugging output. This option is not recommended; it prevents debugging and most performance analysis capabilities. |