SPRUI04E July 2015 – January 2023
Following are assembler options that you can use with the compiler. For more information, see the TMS320C6000 Assembly Language Tools User's Guide.
--asm_define=name[=def] | Predefines the constant name for the assembler; produces a
.set directive for a constant or an .arg directive for a string. If
the optional [=def] is omitted, the name is set to 1.
If you want to define a quoted string and keep the quotation marks,
do one of the following:
|
--asm_dependency | Performs preprocessing for assembly files, but instead of writing preprocessed output, writes a list of dependency lines suitable for input to a standard make utility. The list is written to a file with the same name as the source file but with a .ppa extension. |
--asm_includes | Performs preprocessing for assembly files, but instead of writing preprocessed output, writes a list of files included with the #include directive. The list is written to a file with the same name as the source file but with a .ppa extension. |
--asm_listing | Produces an assembly listing file. |
--asm_undefine=name | Undefines the predefined constant name. This option overrides any --asm_define options for the specified name. |
--asm_cross_reference_listing | Produces a symbolic cross-reference in the listing file. |
--include_file=filename | Includes the specified file for the assembly module; acts like an .include directive. The file is included before source file statements. The included file does not appear in the assembly listing files. |
--machine_regs | Displays reg operands as machine registers in the assembly file for debugging purposes. |
--no_compress | Prevents compression in the assembler. Compression changes 32-bit instructions to 16-bit instructions, where possible/profitable. |
--no_reload_errors | Turns off all reload-related loop buffer error messages in assembly code. |
--strip_coff_underscore | Aids in transitioning hand-coded assembly from COFF to EABI. Although the COFF output is no longer supported, this option remains available as a COFF ABI to ELF EABI migration aid. For COFF ABI, the compiler prepended an underscore to the beginning of all C/C++ identifiers. For EABI, the link-time symbol is the same as the C/C++ identifier name. This option removes the underscore prefix from legacy symbol references as needed. |