ZHCST39A December 2022 – September 2023 AFE11612-SEP
PRODUCTION DATA
In the AFE11612-SEP, the DAC channels can only be set to a positive voltage-output range (0 V to 5 V).
The maximum DAC output for each group cannot be greater than the corresponding AVCC voltage. In all-positive DAC range mode, the AVCC1 and AVCC2 pins must be connected to a positive supply voltage; however these pins are not required to be tied to the same potential. Typically, the positive voltage at each of these pins is dictated by the desired positive-voltage output range, but this configuration is not required.