SLUUCW9 December 2023 BQ76972
Command | Name | Access | Description |
---|---|---|---|
0x000E | EXIT_DEEPSLEEP | Sealed: W Unsealed: W Full Access: W | Exit DEEPSLEEP mode |
0x000F | DEEPSLEEP | Sealed: W Unsealed: W Full Access: W | Enter DEEPSLEEP mode. Must be sent twice in a row within 4s to take effect |
0x0010 | SHUTDOWN | Sealed: W Unsealed: W Full Access: W | Start SHUTDOWN sequence. Must be sent twice in a row within 4s to take effect if sealed. If sent twice while unsealed, the shutdown delays are skipped. |
0x0012 | RESET | Sealed: — Unsealed: W Full Access: W | Resets the device |
0x001C | PDSGTEST | Sealed: — Unsealed: W Full Access: W | In FET Test mode, toggle the PDSG FET enable. |
0x001D | FUSE_TOGGLE | Sealed: — Unsealed: W Full Access: W | Toggle FUSE state |
0x001E | PCHGTEST | Sealed: — Unsealed: W Full Access: W | In FET Test mode, toggle the PCHG FET enable. |
0x001F | CHGTEST | Sealed: — Unsealed: W Full Access: W | In FET Test mode, toggle the CHG FET enable. |
0x0020 | DSGTEST | Sealed: — Unsealed: W Full Access: W | In FET Test mode, toggle the DSG FET enable. |
0x0022 | FET_ENABLE | Sealed: — Unsealed: W Full Access: W | Toggle FET_EN in Manufacturing Status. FET_EN = 0 means FET Test Mode. FET_EN = 1 means Firmware FET Control. |
0x0024 | PF_ENABLE | Sealed: — Unsealed: W Full Access: W | Toggle PF_EN in Manufacturing Status |
0x0030 | SEAL | Sealed: — Unsealed: W Full Access: W | Places the device in SEALED mode |
0x0082 | RESET_PASSQ | Sealed: W Unsealed: W Full Access: W | Resets the integrated charge and timer. Charge resets to 0.5 userAh so that the integer portion is rounded. |
0x008A | PTO_RECOVER | Sealed: W Unsealed: W Full Access: W | Triggers recovery from a Precharge Timeout (PTO) safety event. This also resets the timeout timer for an ongoing precharge cycle. |
0x0090 | SET_CFGUPDATE | Sealed: — Unsealed: W Full Access: W | Enters CONFIG_UPDATE mode |
0x0092 | EXIT_CFGUPDATE | Sealed: W Unsealed: W Full Access: W | Exits CONFIG_UPDATE mode. This also clears the Battery Status()[POR] and Battery Status()[WD] bits. |
0x0093 | DSG_PDSG_OFF | Sealed: W Unsealed: W Full Access: W | Disables DSG and PDSG FET drivers |
0x0094 | CHG_PCHG_OFF | Sealed: W Unsealed: W Full Access: W | Disables CHG and PCHG FET drivers |
0x0095 | ALL_FETS_OFF | Sealed: W Unsealed: W Full Access: W | Disables CHG, DSG, PCHG, and PDSG FET drivers |
0x0096 | ALL_FETS_ON | Sealed: W Unsealed: W Full Access: W | Allows all four FETs to be on if other safety conditions are met. This clears the states set by the DSG_PDSG_OFF, CHG_PCHG_OFF, and ALL_FETS_OFF commands. |
0x0099 | SLEEP_ENABLE | Sealed: W Unsealed: W Full Access: W | Enable SLEEP mode. The default is loaded from data memory, after which this command can change the setting. |
0x009A | SLEEP_DISABLE | Sealed: W Unsealed: W Full Access: W | Disable SLEEP mode. The default is loaded from data memory, after which this command can change the setting. |
0x009B | OCDL_RECOVER | Sealed: W Unsealed: W Full Access: W | Recovers Overcurrent in Discharge Latch (OCDL) in the next execution of the safety engine (about 1 second) |
0x009C | SCDL_RECOVER | Sealed: W Unsealed: W Full Access: W | Recovers Short Circuit in Discharge Latch (SCDL) in the next execution of the safety engine (~1 second) |
0x009D | LOAD_DETECT_RESTART | Sealed: W Unsealed: W Full Access: W | Restarts the timeout on the Load Detect (LD) pin current source if it has already triggered |
0x009E | LOAD_DETECT_ON | Sealed: W Unsealed: W Full Access: W | Force the Load Detect (LD) pin current source to be ON. This command has no effect when the device is configured for autonomous control of the current source (Protections:Load Detect:Active Time > 0). |
0x009F | LOAD_DETECT_OFF | Sealed: W Unsealed: W Full Access: W | Force the Load Detect (LD) pin current source to be OFF. This command has no effect when the device is configured for autonomous control of the current source (Protections:Load Detect:Active Time > 0). |
0x2800 | CFETOFF_LO | Sealed: W Unsealed: W Full Access: W | Drive the CFETOFF pin to a low state if it is configured as a GPO |
0x2801 | DFETOFF_LO | Sealed: W Unsealed: W Full Access: W | Drive the DFETOFF pin to a low state if it is configured as a GPO |
0x2802 | ALERT_LO | Sealed: W Unsealed: W Full Access: W | Drive the ALERT pin to a low state if it is configured as a GPO |
0x2806 | HDQ_LO | Sealed: W Unsealed: W Full Access: W | Drive the HDQ pin to a low state if it is configured as a GPO |
0x2807 | DCHG_LO | Sealed: W Unsealed: W Full Access: W | Drive the DCHG pin to a low state if it is configured as a GPO |
0x2808 | DDSG_LO | Sealed: W Unsealed: W Full Access: W | Drive the DDSG pin to a low state if it is configured as a GPO |
0x2810 | CFETOFF_HI | Sealed: W Unsealed: W Full Access: W | Drive the CFETOFF pin to a high state if it is configured as a GPO |
0x2811 | DFETOFF_HI | Sealed: W Unsealed: W Full Access: W | Drive the DFETOFF pin to a high state if it is configured as a GPO |
0x2812 | ALERT_HI | Sealed: W Unsealed: W Full Access: W | Drive the ALERT pin to a high state if it is configured as a GPO |
0x2816 | HDQ_HI | Sealed: W Unsealed: W Full Access: W | Drive the HDQ pin to a high state if it is configured as a GPO |
0x2817 | DCHG_HI | Sealed: W Unsealed: W Full Access: W | Drive the DCHG pin to a high state if it is configured as a GPO |
0x2818 | DDSG_HI | Sealed: W Unsealed: W Full Access: W | Drive the DDSG pin to a high state if it is configured as a GPO |
0x2857 | PF_FORCE_A | Sealed: W Unsealed: W Full Access: W | First part of two-word command to force the command-based PF. Must be followed by PF_FORCE_B within 4s with no writes in between |
0x29A3 | PF_FORCE_B | Sealed: W Unsealed: W Full Access: W | Second part of two-word command to force the command-based PF. Must be preceded by PF_FORCE_A within 4s with no writes in between |
0x29BC | SWAP_COMM_MODE | Sealed: — Unsealed: W Full Access: W | Change to the communications mode previously configured by changing Settings:Configuration:Comm Type in CONFIG_UPDATE_MODE |
0x29E7 | SWAP_TO_I2C | Sealed: — Unsealed: W Full Access: W | Select I2C Fast mode (Settings:Configuration:Comm Type = 8) in data memory and immediately start using I2C |
0x7C35 | SWAP_TO_SPI | Sealed: — Unsealed: W Full Access: W | Select SPI with CRC mode (Settings:Configuration:Comm Type = 16) in data memory and immediately start using SPI |
0x7C40 | SWAP_TO_HDQ | Sealed: — Unsealed: W Full Access: W | Select HDQ using ALERT pin mode (Settings:Configuration:Comm Type = 3) in data memory and immediately start using HDQ |