SWRU473A February 2017 – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
The terminal can also be used for debug messages. The default configuration is 115200 bps, 8 bits, no parity, and 1 stop bit. Most of the debug messages are self-explained. For better tracking, each message is preceded by the task and module generating the message enclosed in brackets.
Table 3 lists some common messages to help users track the application status.
| Message | What Does it Mean? |
|---|---|
| [Provisioning task] Provisioning Started. Waiting to be provisioned..!! | The CC3220 is in provisioning mode. The user must use the SimpleLink Wi-Fi Starter Pro application to provision the device. |
| [ProvisioningEvent] Connection to AP succeeded | During provisioning, the CC3220 managed to decode the AP credentials and connect to it successfully. |
| [ProvisioningEvent] Confirmation Success! | During provisioning, the CC3220 supplied feedback to the SimpleLink Wi-Fi Starter Pro application. |
| [Provisioning task] Provisioning completed successfully..! | Provisioning completed successfully. |
| [ProvisioningEvent] Provisioning stopped | Provisioning is stopped, which may indicate the following:
|
| [Provisioning task] committing new OTA download... | Upon end of OTA procedure, indicates a new software package is being committed. |
| [Provisioning task] commit succeeded | New OTA software package committed successfully. |
| [Provisioning task] Rollback error sl_FsCtl | New OTA software package failed its validation testing (connect to AP while in Station mode or initialize while in AP mode), reverting to previous software package. |
| [Provisioning task] failed to commit new download, reverting to previous copy by resetting the device | New OTA software package failed to commit, reverting to previous software package. |
| Return To Factory Image successful. Do a power cycle (POR) of the device using switch SW1-Reset | After a return-to-factory is triggered and the device is up, a manual reset is required from the user to complete the operation. |
| Connection Success (feedback to Smartphone app failed) | During provisioning, the CC3220 connected to the AP successfully, but failed to supply feedback to the SimpleLink Wi-Fi Starter Pro application. |
| [Link local task] HTTP GET Request | Indicates client HTTP GET request. For details see Table 4. |
| [Link local task] characteristic is: | During HTTP request, indicates the relevant resource. |
| [Link local task] HTTP POST Request | Indicates client HTTP POST request. For details see Table 4. |
| [Link local task] value is: | During HTTP request, indicates the value of the resource. |
| [Link local task] HTTP PUT Request | Indicates client HTTP PUT request. For details see Table 4. |
| [Link local task] Received OTA filename | Archive filename received during the OTA update. Filename and file size follows. |
| [Link local task] OTA filename is in *.tar format | Archive filename received during the OTA update is not in tar format. |
| [Link local task] OTA bundle version file does not exist | OTA version file does not exist on the file system. This is informative, not an error. |
| [OtaArchive_CheckVersion] accept the new version | OTA version file does not exist on the file system. New version is accepted. Version number follows. |
| [OtaArchive_CheckVersion] newer version update | New OTA version is newer than the stored version. |
| [OtaArchive_CheckVersion] older version update | New OTA version is older than the stored version. |
| [OtaArchive_RunParseTar] Create/Open for write file | File is updated on file system during the OTA update. Filename follows. |
| [OtaArchive_RunParseTar] Downloading File Completed | File has been downloaded and updated on file system successfully during the OTA update. |
| [OTA report task] OTA progress | The status of the progress bar displays in percentages during the OTA update. |
| [Link local task] sl_extLib_OtaRun: — Download file completed | OTA procedure completed successfully. |
| [Link local task] sl_NetAppRecv error | Error in communication with the client during the OTA update. Error code follows. |
| [Link local task] OtaArchive error | Error in the archive module during the OTA update. Error code follows. For details refer to the OtaArchive.h header file. |
| [Control task] switching to AP mode | The CC3220 is switching to AP mode. |
| [Control task] device not started in AP role | Configuring the CC3220 as AP failed. |
| [Control task] device started in AP role, rebooting device... | Switching to AP mode succeeded, rebooting application. |
| [Control task] device cannot start in AP mode, please reset the board | Switching to AP mode failed. Manual reset is required. |
| [ERROR] - FATAL ERROR | Fatal error occurred. Manual reset is required. |