SWRU473A February   2017  – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF

 

  1.   SimpleLinkrep%#8482; Wi-Fi® CC3220 Out-of-Box Application
    1.     Trademarks
    2. 1 Introduction
    3. 2 Download and Installation
    4. 3 Installation for Basic Users
      1. 3.1 UniFlash
      2. 3.2 SimpleLink™ Wi-Fi® Starter Pro Mobile Application
      3. 3.3 Serial Terminal
      4. 3.4 XDS110 Driver Installation
    5. 4 Building the Setup
    6. 5 Flashing the Out-of-Box Project
    7. 6 Getting Started With the OOB Demonstration
      1. 6.1 Connecting to the CC3220
        1. 6.1.1 CC3220 Provisioning
        2. 6.1.2 CC3220 as AP
      2. 6.2 Browse Onboard Website
        1. 6.2.1 Local Network Demo
        2. 6.2.2 OTA Update
        3. 6.2.3 Advanced Settings
      3. 6.3 Using the Mobile Application
        1. 6.3.1 Connect to the CC3220
        2. 6.3.2 Local Network Demo
        3. 6.3.3 OTA Update
          1. 6.3.3.1 Local OTA When CC3220 is in AP Mode
      4. 6.4 Returning to Factory Image
    8. 7 Troubleshooting
      1. 7.1 Red LED Legend
      2. 7.2 Extra Debugging
      3. 7.3 Terminal Messages
    9. 8 Limitations and Known Issues
    10. 9 Out-of-Box for Advance Users
      1. 9.1 Installations for Advance Users
        1. 9.1.1 CC3220 Software Development Kit (SDK)
        2. 9.1.2 Service Pack
        3. 9.1.3 CCS IDE
          1. 9.1.3.1 Add CCS Support for FreeRTOSv9
          2. 9.1.3.2 Product Settings Verification
      2. 9.2 Source Files Briefly Explained
      3. 9.3 Building the OOB Project Using CCS
        1. 9.3.1 Executing in Debug Mode
        2. 9.3.2 Program a User Modified OOB Binary
  2.   Revision History

Red LED Legend

This section lists all state options of the red LED (D7). The red LED (D7) indication can help users understand the application flow, and debug cases where the application does not behave as expected. Only the red LED (D7) is used for status indication, and similar indications may be applied in more than one occasion. To distinguish similar indications, the user must be aware of the executed procedure. Table 2 lists all options.

Table 2. LED Indication Legend

Red LED indication Procedure Interpretation
Blinking once per 2 seconds Provisioning CC3220 is being provisioned.
Solidly on Provisioning Connection to the AP is up.
Solidly off Provisioning Connection to the AP is down.
Blinking once per second Local network connection For Station mode, connection to the AP is in progress. For AP mode, initialization is in progress.
Solidly on Local network connection For Station mode, connection to the AP is up. For AP mode, initialization is done.
Solidly off Local network connection Applies in Station mode only. Connection to the AP is down.
Blinking 5 times per second OTA update OTA update of the CC3220 is in progress.
Solidly on OTA update OTA update of the CC3220 succeeded.
Solidly off OTA update OTA update of the CC3220 failed.
Blinking once per second Return to default Return to default procedure is done. Waiting for the user to manually restart the CC3220 LaunchPad