SWRU473A February   2017  – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF

 

  1.   SimpleLinkrep%#8482; Wi-Fi® CC3220 Out-of-Box Application
    1.     Trademarks
    2. 1 Introduction
    3. 2 Download and Installation
    4. 3 Installation for Basic Users
      1. 3.1 UniFlash
      2. 3.2 SimpleLink™ Wi-Fi® Starter Pro Mobile Application
      3. 3.3 Serial Terminal
      4. 3.4 XDS110 Driver Installation
    5. 4 Building the Setup
    6. 5 Flashing the Out-of-Box Project
    7. 6 Getting Started With the OOB Demonstration
      1. 6.1 Connecting to the CC3220
        1. 6.1.1 CC3220 Provisioning
        2. 6.1.2 CC3220 as AP
      2. 6.2 Browse Onboard Website
        1. 6.2.1 Local Network Demo
        2. 6.2.2 OTA Update
        3. 6.2.3 Advanced Settings
      3. 6.3 Using the Mobile Application
        1. 6.3.1 Connect to the CC3220
        2. 6.3.2 Local Network Demo
        3. 6.3.3 OTA Update
          1. 6.3.3.1 Local OTA When CC3220 is in AP Mode
      4. 6.4 Returning to Factory Image
    8. 7 Troubleshooting
      1. 7.1 Red LED Legend
      2. 7.2 Extra Debugging
      3. 7.3 Terminal Messages
    9. 8 Limitations and Known Issues
    10. 9 Out-of-Box for Advance Users
      1. 9.1 Installations for Advance Users
        1. 9.1.1 CC3220 Software Development Kit (SDK)
        2. 9.1.2 Service Pack
        3. 9.1.3 CCS IDE
          1. 9.1.3.1 Add CCS Support for FreeRTOSv9
          2. 9.1.3.2 Product Settings Verification
      2. 9.2 Source Files Briefly Explained
      3. 9.3 Building the OOB Project Using CCS
        1. 9.3.1 Executing in Debug Mode
        2. 9.3.2 Program a User Modified OOB Binary
  2.   Revision History

CC3220 as AP

When the SimpleLink Wi-Fi Starter Pro application is not available, the user can set the CC3220 as an AP, and connect to it directly. Setting the CC3220 as an AP is very convenient when no AP is available. AP mode is applied by pressing the SW2 switch on the CC3220 LaunchPad. The terminal shows the Switching to AP Mode message, followed by a message indicating the IPv4 address of the CC3220 server.

To connect to the CC3220, the user must look for a network name that begins with mysimplelink-xxyyzz in which xxyyzz stands for the 3 least significant bytes of the unique MAC address of the CC3220. Successful connection to the CC3220 is indicated in the terminal where the MAC address, and the IP address of the connected station are presented.

Configuring the CC3220 in AP mode is not persistent, which means that manual reset of the board makes the CC3220 return to its default, configure as Station mode, and try to connect to a stored profile. If unsuccessful, the CC3220 is configured in provisioning mode. The only time AP is persistent is upon automated reset of the CC3220, which occurs as part of the OTA update procedure.